AXIS#.MOTOR.TBRAKEAPP
Description
This parameter is the mechanical delay required for the motor brake to close. When disabling an axis, the drive will servo to hold position for this time delay, allowing the brake to apply.
-
-
If AXIS#.MOTOR.AUTOSET = 1 and motor memory version is 0.2 or greater, this parameter will be automatically configured for Kollmorgen motors.
Context
For more information see Brake and Motor.
Versions
Action | Version | Notes |
---|---|---|
Implemented | 02-00-00-000 |
General Information
Type |
Read/Write |
Units |
ms |
Range |
0 to 1,000 ms |
Default Value |
75 ms |
Data Type |
Integer |
See Also |
N/A |
Stored in Non Volatile Memory |
Yes |
Variants Supported
All variants are supported.
Fieldbus Information
FieldbusA Fieldbus is an industrial network system for real-time distributed control (e.g. CAN or Profibus). It is a way of connecting instruments in a plant design | Parameter | Index | Sub-Index | Data Type | Float Scale | Units | Access | PDOPDO is a type of protocol frame used in some fieldbuses. A PDO contains one or more object dictionary entries, which define the application data transferred between devices. Mappable |
---|---|---|---|---|---|---|---|---|
EtherCAT***EtherCAT is an open, high-performance Ethernet-based fieldbus system. The development goal of EtherCAT was to apply Ethernet to automation applications which require short data update times (also called cycle times) with low communication jitter (for synchronization purposes) and low hardware costs COE and CANopen | AXIS1.MOTOR.TBRAKEAPP | 0x500B | 0x1A | UINT | - | - | RW | False |
AXIS2.MOTOR.TBRAKEAPP | 0x510B | 0x1A | UINT | - | - | RW | False |